Kantech integrates Aperio wireless lock technology with EntraPass 7.0

Share On
Share

Aperio Wireless Lock

WESTFORD, MA. July 11, 2016 –– Tyco Security Products introduces the integration of ASSA ABLOY Aperio® Wireless Lock Technology with all editions of Kantech EntraPass Security Software 7.0, for a fully integrated and managed lock solution that expands access control to include nearly any door or opening in a facility, enabling incremental wireless lock deployment.

When integrated with EntraPass 7.0 Security Software, ASSA ABLOY Aperio Wireless Lock Technology offers an affordable way to bring the flexibility of wireless lock technology to any door in a facility, including cabinets, drawers and server racks in settings such as universities, pharmacies, hospitals, human resources departments, data centers and any other door where electronic access control was previously cost prohibitive. Aperio Wireless Lock Technology offers the same real-time communication common to traditional access control systems, but also can be installed or retrofitted in existing facilities with little to no operational disruption.

With the integration, ASSA ABLOY Aperio Wireless Locks become part of the EntraPass security software eco-system and can be managed from the EntraPass interface for a unified security management experience, controlling core functions such as managing events, reporting and integrated mapping. A hardwired connection enables reliable communications between the Aperio hub and state-of-the-art Kantech KT-1-M and KT-400 door controller, which controls decisions on the locks. Wireless connectivity, secured with 128-bit AES encryption, connects the locks back to the Aperio hub.

The KT-1-M door controller can support a wired full-one-door configuration or two additional wireless locks with an additional software license purchase. Similarly, the KT-400 door controller can support eight additional wireless locks beyond its standard wired full-four-doors, also with the addition of software licenses.

“The Kantech ethos centers on delivering cutting-edge technologies to the small to medium business market, while also providing this market the freedom to expand their businesses and operations at their own speed,” said Jason Ouellette, Product Line Director – Access Control, Tyco Security Products. “The integration between ASSA ABLOY Aperio Wireless Lock Technology and EntraPass 7.0 Security Software marries the flexibility and affordability of wireless lock technology with the advanced security management and intuitive user interface of EntraPass 7.0.”

The ASSA ABLOY Aperio Wireless Locks supported by the integration are ideal for a wide array of environments including mortise, cylindrical, and exit devices for standard doors and an electronic cylinder to replace a traditional mechanical keyed cylinder. Wireless cabinet locks, which can be used for cabinets, lockers and drawers, are well-suited for healthcare facilities for storing equipment, prescriptions, patient files and other valuables, while a server rack lock option improves the security level of data centers and hardware.

For more information, visit Kantech at www.kantech.com.

- End -

About Kantech
Kantech access control solutions are part of the Security Products business unit of Tyco, the world's largest pure-play fire protection and security company. Kantech access control technologies are ready to use right out of the box, and provide solutions that are compact, and easy to use for smaller businesses while scaling to meet the needs of larger businesses. Kantech solutions can easily link to Exacq and American Dynamics video systems and DSC Intrusion panels to provide an integrated, holistic security solution. To learn more about Kantech products, visit www.kantech.com.

 

About Tyco Security Products
Tyco Security Products and its leading brands conduct business in over 177 countries around the world, in multiple languages and employ over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential. Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world's top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities and over five million private residences.

Share On
Share