- Johnson Controls
- Building Insights
- How AI innovations are reshaping facility management
Reach out to take the next step in advancing your operational efficiency
4 ways OpenBlue digital healthcare solutions are helping hospitals optimize critical environments
Contact usHighlights
- Digital healthcare solutions like OpenBlue Operating Room Optimization are transforming patient care through AI, IoT and smart technologies that improve efficiency and safety
- Hospitals adopting connected systems benefit from streamlined operations, better resource management, and enhanced patient experiences
- Investing in data-driven solutions powered by the OpenBlue digital ecosystem positions healthcare organizations for long-term operational resilience and regulatory compliance
Every organization that owns or leases real estate must balance competing priorities of cost control, regulatory compliance and operational resilience. But for hospitals and healthcare systems, the consequences of falling short are uniquely serious.
Across the industry, healthcare systems are adopting smart, data-driven solutions like our OpenBlue suite of digital tools to help move beyond manual processes — unlocking new efficiencies, improving sustainability and enhancing patient outcomes. Smart hospitals are proving that, with the right technology, operational challenges can become powerful drivers of innovation and growth.
Here are four key reasons providers are embracing IoT in healthcare with smart hospital technologies like OpenBlue Operating Room Optimization, from delivering better, AI-driven patient care to improving efficiency and sustainability and more.
1. Minimizing disruptions, delays and costly waste
Detect issues early and act before disruptions impact care.
Automated, real-time monitoring doesn’t just make data gathering and reporting easier; it can also serve as an important safeguard for patient care. Even slight deviations in temperature, humidity or pressure in sensitive areas like ORs, sterile processing rooms and pharmaceutical storage can have costly and disruptive consequences. These include spoiled medications and delayed procedures, which can impact patient safety and outcomes.
With AI-powered fault detection and diagnostics (FDD) capabilities, staff can receive instant alerts when a deviation is detected, helping them take corrective action before issues escalate. The AI agent can also identify potential root causes of the issue, like a malfunctioning component or an improperly adjusted control setting, streamlining troubleshooting and reducing downtime.
These AI-driven patient care capabilities can help support better healthcare outcomes:
- Fewer procedure delays or cancellations, ensuring ORs and critical spaces remain ready even during network outages or other operational disruptions
- Improved safety and compliance since automated monitoring ensures environmental conditions consistently meet regulatory standards
- Reduced waste and improved equipment reliability, which allows clinical staff to focus on patient care rather than operational troubleshooting
The result: The potential for fewer procedure delays or cancellations, improved safety and compliance, reduced waste and improved equipment reliability.
2. Streamlined monitoring and compliance reporting for critical environments
Automate monitoring and documentation to reduce risk and save time.
Of course, ORs aren’t the only critical spaces in a hospital. Laboratories, pharmaceutical storage areas and sterile processing rooms must also adhere to strict environmental conditions and comply with rigorous regulatory and clinical standards.
Ensuring compliance requires continuous monitoring of temperature, humidity and pressure, along with regular reporting to regulatory agencies. However, manual monitoring and reporting are still common, making the process inefficient and prone to human error.
OpenBlue integrates with existing building systems to monitor and document these metrics in real time. Teams gain:
- Instant remote visibility through intuitive dashboards that make it easy to view vital environmental information at a glance.
- Auto-generated compliance reports, reducing staff time behind documentation by up to 75%.
- Automated updates and enhancements that make it easy to stay on top of regulatory changes and quickly determine when space conditions need adjustment to maintain compliance.
The result: Simplified compliance, stronger accuracy and more time for patient-critical work.
See how OpenBlue helped one hospital save $5,000 annually per operating room
3. Driving efficiency and sustainability in surgical operations
Turn operational efficiency into measurable sustainability impact while easing staff workload.
The kind of energy waste reductions Operating Room Optimization can deliver are good for both the business and the planet. By deploying this smart hospital technology, a major healthcare organization reduced energy costs by over $5,000 annually per operating room – a potential savings of $160,000 per year across their campus.
Beyond cost and sustainability benefits, Operating Room Optimization provides valuable analytics on room utilization and performance. Facility and surgical services teams can use these insights to:
- Identify underused ORs and improve scheduling efficiency
- Support strategic growth decisions about where to expand or consolidate surgical capacity
- Align sustainability initiatives with measurable operational outcomes
- Reduce manual documentation and monitoring tasks, allowing staff to focus on higher-value clinical or operational work rather than constantly checking room conditions
The result: A smarter, more agile operating environment that strengthens financial, environmental and workforce performance.
4. A smarter approach to energy use in the operating room
Cut energy waste, reduce manual workloads and maintain compliance through intelligent automation.
Hospital operating margins are under pressure from rising supply and drug costs, which are growing faster than operating revenues. OpenBlue Operating Room Optimization is helping hospitals alleviate some of that pressure by reducing one of their largest controllable expenses: energy.
Hospitals use three times more energy than the average commercial building because so many clinical spaces must maintain strict temperature, humidity and lighting conditions. Operating rooms (OR) are among the most energy-intensive; they consume up to six times more energy per square foot than the hospital overall. Traditionally, hospitals have kept OR HVAC and lighting systems running continuously to maintain surgical standards – even though ORs are typically in use less than 30% of the time.
With digital healthcare solutions like OpenBlue Operating Room Optimization, hospitals can:
- Cut energy waste by automatically adjusting consumption when ORs are idle
- Automatically restore and maintain optimal conditions when procedures are scheduled using smart logic integrated with occupancy sensors and surgery schedules
- Reduce manual checks and adjustments, easing the burden on clinical and facilities staff who are already stretched thin
- Give clinicians visibility and control to verify room status, ensure compliance and manually override automated settings directly from in-room displays or mobile devices
The result: Measurable energy savings, fewer manual tasks, seamless compliance and greater staff confidence in OR readiness.
Optimizing environments for better patient outcomes
Operating rooms and other critical environments in hospitals are central to delivering quality care, but they’re also among the most energy-intensive and risk-sensitive areas of a hospital. In the past, organizations have invested enormous amounts of time, effort and money to ensure these spaces operate within regulatory and clinical standards.
By ensuring optimal environmental conditions, automating compliance, improving space utilization and supporting sustainability goals, hospitals gain significant operational advantages that translate directly into improved patient outcomes, stronger margins and long-term operational resilience. And best of all, OpenBlue solutions integrate seamlessly with existing building and clinical systems, regardless of vendor, so hospitals can leverage their current infrastructure without disruption.
With digital healthcare solutions like OpenBlue supporting critical environments, hospitals can reclaim valuable resources and reinvest them in their core mission.
Reduce costs, operate more sustainably and efficiently and drive business growth with OpenBlue
Frequently Asked Questions
What are OpenBlue digital healthcare solutions, and how do they support hospitals?
OpenBlue digital healthcare solutions from Johnson Controls are a suite of AI‑ and IoT‑powered technologies designed to help hospitals optimize operating rooms and other critical environments. Solutions like OpenBlue Operating Room Optimization use real-time data, automation and analytics to help improve environmental control, ensure regulatory compliance, reduce energy waste and enhance operational efficiency. OpenBlue can enable smarter, more connected hospitals that can improve patient outcomes while strengthening financial and operational resilience.
How do OpenBlue healthcare solutions improve operating room readiness and patient outcomes?
OpenBlue can improve operating room readiness by continuously monitoring temperature, humidity, pressure and occupancy, then automatically adjusting systems to maintain optimal conditions. AI-driven fault detection and diagnostics help identify issues before they cause procedure delays, cancellations, or compliance risks. By keeping ORs and other critical spaces within required standards, even during network or system disruptions, OpenBlue can support safer surgical environments, more reliable scheduling and better overall patient care.
Can OpenBlue integrate with existing hospital systems and equipment?
Yes. OpenBlue digital healthcare solutions are vendor-agnostic and designed to integrate with existing building systems, medical facilities infrastructure and clinical workflows. Hospitals do not need to replace current equipment to benefit from OpenBlue. Instead, they can layer advanced analytics, automation and AI capabilities on top of their existing technology investments, which helps enable a smoother transition to smart hospital operations with minimal disruption to staff or patients.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)