Improving winter heating and energy efficiency across five rail stations in China

Five stations along the Jinan–Zhengzhou High-Speed Railway in Shandong, China required reliable heating to maintain passenger comfort during winter conditions as temperatures dropped to -15°C. The stations set targets to improve heating performance while reducing energy use and emissions.

The upgrade delivered measurable efficiency gains and emissions reductions, supported by an ultra-low temperature heating solution designed for stable, data-driven operation.

Impact Highlights

Sustainability with arrow down icon

3.27 million KwH annual electricity savings

co2

15% energy efficiency improvement

sustainability icon

2,803 tons of CO₂ emissions reduced annually

Addressing heating limitations and operational demands in extreme winter conditions

Winter conditions created significant operational challenges across rail stations in Shandong, China, where temperatures can drop below -15°C. Existing heating systems had limited capacity, and long-distance piping from central networks led to substantial heat loss before reaching indoor spaces.

These constraints resulted in uneven terminal temperatures, higher energy consumption and rising operating costs. At the same time, large waiting halls, high ceilings and heavy passenger traffic increased heating demand and added complexity to system performance.

With strict reliability requirements and limited tolerance for disruption, the stations needed to maintain stable heating to support uninterrupted operations and deliver consistent indoor temperatures, around 20°C, for passenger comfort. At the same time, in line with China’s dual-carbon goals, the stations required a solution that could reduce emissions while delivering stable, efficient and cost-effective operation.

Advanced heating systems designed for extreme cold and continuous operation

An ultra-low temperature heating solution using YORK air-source heat pumps was implemented across the stations to address winter heating challenges, enabling reliable performance in extreme cold conditions.

To meet varying heating demands across large, high-traffic station environments, the solution uses a modular design comprising 44 units. This allows system capacity to be scaled and configured across different areas, helping match heating demand while improving overall efficiency.

Zone-level control further supports consistent indoor temperatures, reducing unnecessary energy use while maintaining passenger comfort across different station spaces.

To ensure stable operation in harsh winter conditions, the system incorporates advanced features such as intelligent defrost control, dual refrigeration circuits and staged defrost operation. These capabilities help maintain consistent heating performance and support continuous operation even during extreme weather.

A comprehensive validation process, including low-temperature testing, frost and defrost cycles, and stress testing under extreme conditions, helps ensure long-term reliability and durability across complex rail environments.

Improved reliability, energy efficiency and passenger comfort

Following implementation across five stations, heating performance improved significantly, enabling stable indoor conditions throughout extreme winter weather. The upgraded system supports reliable operation while delivering consistent passenger comfort and improved energy performance.

Enhanced system control and modular operation enable operators to maintain stable heating while optimizing energy use. These capabilities improve operational reliability, reduce energy consumption and contribute to lower operating costs.

Passengers experience consistent waiting hall temperatures during peak travel periods and harsh winter conditions, improving comfort across high-traffic station environments.

Key outcomes include:

  • 3.27 million kWh of electricity saved annually
  • 15% improvement in energy efficiency
  • 2,803 tons of CO₂ emissions reduced annually (equivalent to the carbon absorption around 150,000 trees)

About Ji’nan-Zhengzhou High-Speed Railway

The Ji’nan–Zhengzhou High-Speed Railway in China is a 407 km high-speed corridor designed to improve regional mobility and connectivity. Built for speeds of up to 350 km/h, the line reduces end-to-end travel time to approximately 1.5 hours.

As part of China’s national high-speed rail network, the corridor supports faster movement of people and economic activity across key north–south and east–west routes.

Building Insights

The one-stop shop for smart buildings news and insights

Take a look

About the facility

  • Five stations along the Jinan–Zhengzhou High-Speed Railway in China
  • Located in the Shandong section, with demanding winter climate conditions
  • Part of China’s national high-speed rail network

Solutions:

Share

Similar stories

Ship on water

Inside MCIA’s unified approach to smarter airport operations

Mactan-Cebu International Airport modernized and unified its BAS to streamline operations, lower energy use, and improve system visibility across both terminals.

federal facility

Federal facility drives 12% potential savings with smarter chilled water plant performance

Federal facility achieves 4.5% actual energy efficiency gains, saving nearly 190,000 kWh annually while supporting net zero goal.

Building

Graha CIMB Niaga improves energy efficiency in Jakarta

Across its 30,000 m² tower, Graha CIMB Niaga achieves measurable energy savings. With Metasys centralizing HVAC control, the officer tower boosts transparency and streamlines daily operations.

Global Consulting Company

Global consulting firm sees 17% energy savings and reduces CO2 emissions

Company realizes significant financial impact while improving air quality, occupancy comfort and productivity.

Contact us

Please read our Privacy Notice for information on how we protect and manage your personal data. By completing this form and submitting your information, you confirm that you have reviewed, understood and accepted our privacy terms as well as our cookie terms.