- Johnson Controls
- Customer Success Stories
- National Museum of Anthropology
Protecting Mexico’s cultural heritage through advanced fire safety systems
Safeguarding a world-renowned museum with fire detection and suppression solutions
Impact Highlights
Comprehensive fire detection coverage across approximately four hectares
Clean-agent fire suppression for sensitive collection
Protection of more than 600,000 cultural artifacts
Protecting irreplaceable cultural heritage from fire risk
The National Museum of Anthropology in Mexico City is one of the most important cultural institutions in Latin America, housing more than 600,000 archaeological, ethnographic, and anthropological objects. Protecting this irreplaceable collection from fire risk was essential to preserving the museum’s legacy and ensuring visitor safety.
Given the value and sensitivity of the artifacts, the museum required a fire protection strategy that would deliver early detection and effective suppression without damaging collections. The project also needed to comply with regulatory requirements and adapt to the museum’s large, open spaces and diverse risk areas. Johnson Controls worked closely with the museum’s Museography, Restoration, and Security teams to assess needs and define the optimal solution.
Integrated fire detection and suppression tailored to a museum environment
Johnson Controls designed and implemented a comprehensive fire safety solution to protect the National Museum of Anthropology’s extensive and highly sensitive collections. The approach combined early detection, targeted suppression, and centralized monitoring to reduce fire risk while preserving valuable artifacts.
The solution included:
- Simplex® fire alarm and detection system with approximately 1,600 devices, including detectors, manual stations, strobe lights, and specialized technologies such as Photobeam for large, open areas
- Two Simplex 4100 control panels providing centralized oversight and continuous monitoring across the museum’s facilities
- Fire suppression systems installed in 24 specific areas, selected based on the risk profile and sensitivity of each space
- Ansul® SAPPHIRE clean-agent systems to protect libraries and vaults without damaging artifacts or emitting harmful substances
- CO₂-based suppression systems in electrical and mechanical rooms to control fires without harming critical equipment
Together, these systems provide comprehensive protection across the museum’s four-hectare site while supporting regulatory compliance, rapid response, and the long-term preservation of Mexico’s cultural heritage.
“Thanks to Johnson Controls and the Board of Trustees, the installation of this first-class equipment in the National Museum of Anthropology became a reality we needed for peace of mind.”
Armando Arbide
Assistant Safety Director, National Museum of Anthropology
Through the implementation of advanced fire detection and suppression systems, the National Museum of Anthropology achieved a new level of protection for its cultural heritage. The solution strengthened safety, improved responsiveness, and reduced the risk of damage or loss to priceless artifacts.
Key outcomes include:
- Continuous fire surveillance across approximately four hectares of museum space
- Accurate and rapid fire detection, improving response times and internal communication
- Targeted suppression in critical areas, protecting libraries, vaults, and technical rooms without harming artifacts
- Improved regulatory compliance and reduced risk of economic loss
About The National Museum of Anthropology
About the facility
- Mexico City, Mexico
- Over 2.6 million visitors annually
- More than 600,000 archaeological, ethnographic, and anthropological objects
Solutions:
Similar stories
Fire Protection for Frasers Group’s Automated Warehouse
Frasers Group implemented a bespoke fire detection and extinguishment system to safeguard its 13,000 m² automated warehouse and maintain operational continuity.
Fire Safety Fit-Out for Birmingham’s Tallest Office Building
103 Colmore Row partnered with Johnson Controls to deliver a compliant fire suppression fit-out for Birmingham’s tallest office building on time and within budget.
Custom Fire Protection Solutions Deliver Significant Economic and Operational Benefits
Johnson Controls partners with a global retailer to upgrade fire protection systems across thousands of stores with minimal operational disruption
Modernizing security at America’s most beloved ballpark
Johnson Controls designed a comprehensive security solution that addresses Fenway Park’s unique combination of security needs, operational efficiency goals and historical preservation requirements. The implementation centers on the Connected Security Services, full infrastructure upgrades and a collaborative maintenance partnership.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)