7 min read
April 17, 2026

Share

Highlights

  • Adopting a robust data center facility security strategy is paramount to a data center’s long-term resilience and viability
  • Defense in depth is seen as the optimal strategy for overcoming the security challenges faced by modern data centers
  • Each of the layers within a defense in depth strategy provides overlapping protection and removes possible overreliance on any individual security control

At the core of all online operations, data centers support critical infrastructure and power everything from cloud services, global finance and ecommerce to AI applications, healthcare and worldwide communications. This reality calls for an integrated approach of both cyber and physical security for data centers. That starts with the physical space itself - a space that houses thousands of servers, storage systems, networking systems and potentially high-value or sensitive data. And for that reason, when it comes to a data center’s long-term viability and resilience, physical security is paramount. It is even intrinsically linked to online protection. In fact, according to the “IBM Cost of Data Breach Report 2025,” nearly 1 in 10 data breaches start with a physical security compromise.

While having a robust cybersecurity strategy is vital for protecting these critical environments, a comprehensive physical security program must be designed, implemented, monitored and managed. The servers, the data they process and the buildings that house them need to be protected from physical threats such as break-ins, vandalism, arson, theft of sensitive information or unauthorized access to high-risk areas.

Each data center layer presents unique vulnerabilities that require overlapping precautions

Addressing the security challenges of a modern data center

As data centers have increased in scale and complexity, so too have the physical security challenges that go along with them. While effective management of insider and outsider threats remains a top priority, today’s expectations demand solutions that allow security operators to spend less time on manual processes – such as threat hunting and incident forensics across multiple tools and compliance reporting – and more time on investigating prioritized incidents and executing orchestrated responses.

Given the fluctuations in size and scale of data centers, security requirements can vary widely from location to location. However, whether they are hyperscalers, colocators or large enterprises, all data centers share some common physical security challenges.

These include:

1. Optimizing perimeter protection to maximize coverage and reduce false alarms
2. Implementing different levels of access to staff, contractors and visitors
3. Recognizing and tracking vehicles, people and objects as they move around the facility to spot behavioral and occupancy anomalies – especially near core assets
4. Strengthening access to high-risk areas with multi-factor authentication
5. Compiling event data across security systems to effectively detect malicious behavior

Addressing these challenges and protecting these critical facilities requires more than isolated safeguards. It demands an integrated, multi-layered approach that anticipates and helps neutralize threats before they impact operations and disrupt business continuity.

Or, more specifically, an optimal facility security approach requires defense in depth.

The layers of our defense in depth strategy

5 essential layers of a strong, defense in depth strategy

Defense in depth is a comprehensive security strategy that uses multiple, layered security controls and technologies to protect assets at every level of data center access.

With a layered defense in depth approach to security, data center operators and facility managers can protect the data center from the outside in. The approach starts at the outermost boundaries, where strong fencing controls and intelligent cameras protect the perimeter. The layered protection continues as you move inward from building and common areas to the most sensitive locations and assets. All layers are then brought together in a central security operations platform.

 

Below is a breakdown of the five layers of protection that are used in this approach.

1. Perimeter protection - the first line of defense

Starting at the outer bounds of a facility, the first layer of protection is where you spot potential intruders as they approach or enter the surrounding premises. Intelligent camera systems can identify and track people, objects, vehicles and license plates, while ground-based radar covers blind spots.

Together, these tools aim to provide a comprehensive view of activity around the premises. Integrated intrusion detection and access control systems further bolster this line of defense and give operators early warnings so that they can stop unauthorized access before threats reach the building.

2. Monitoring entrants to building and common areas

Once on the premises, focus shifts to providing secure building access and monitoring movement through lobbies, corridors and shared spaces. These areas act as gatekeepers to any structure, and it is no different within a data center facility. Credential-based entry, biometric authentication and visitor management systems mean only authorized personnel can gain access to a building or common area.

Be they one-off visitors or established employees, every entrant must be accounted for at all times. Real-time monitoring and camera systems can track movement and maintain visibility of personnel throughout the facility. This is essential for spotting behavioral anomalies and suspicious activities as soon as they occur.

3. Protecting infrastructure zones and technicals areas

If critical assets are held at the core of the facility, then the margin for error becomes smaller as you move inward – and the price for having a vulnerability becomes more severe. Arson, sabotage and other forms of vandalism can have a detrimental impact on operations. Even accidental damage caused by underqualified personnel can come with serious consequences.

This third critical layer includes mechanical rooms, electrical panels and network closets. These areas require restricted access protocols, environmental monitoring systems and centrally controlled electronic locks. Centralized implementations and enforcement of granular, role-based access control means that only approved staff can enter to reduce risks of both accidental breakages and malicious activities.

4. Securing high-risk areas and critical assets

The final core layer – which includes server rooms, racks and data vaults – demands the highest level of security. Multi-factor authentication, cabinet-level locking systems and continuous surveillance can safeguard your most sensitive assets.

At this layer, every access attempt is logged and alerts are triggered for unauthorized activity. This allows for rapid response and forensic analysis.

5. Bringing it all together with security operations

All components and enforcement points are centrally monitored from a security operations platform. Centralized monitoring and event correlation provide a complete picture of potential threats and allow data center personnel to effectively orchestrate faster, more appropriate responses. This integration also simplifies compliance and audit processes, while ensuring event logs are stored for post-incident investigations.

With a robust defense in depth strategy, threats can be deterred, detected and mitigated at multiple junctures. Each layer of protection plays its own vital role in reducing risk and enhancing operational security. Each layer serves a purpose, plays a part in overcoming a specific security challenge and adds to the overall resilience of the facility. Together, each layer creates an integrated and holistic security system with overlapping protection removing any possible overreliance of a single control.

Data center facility security from Johnson Controls

Johnson Controls has been implementing this defense in depth approach in some of the most complex critical environments. Check out our range of solutions that will help you protect your data center at every layer, from tracking movements at the outer perimeter to securing the highest risk areas at the core of your facility.

Build layers of defense with Johnson Controls

Learn more

FAQs

What is data center facility security?

Data center facility security includes all the physical processes, technologies and policies used to secure the physical data center location and the assets within it.

What are the key components of a robust data center physical security system?

A robust data center physical security system takes a multi-layered defense in depth approach to protecting every area of the data center – from the outer boundaries to individual server cabinets.

Key components of a robust data center physical security system include:

  • Perimeter protection
  • Intelligent video surveillance cameras
  • License plate, person and object recognition
  • Access control and security management systems
  • Credential and biometric based entry
  • Environmental monitoring systems
  • Centrally controlled electronic locks

What is defense in depth for data centers?

Defense in depth is a comprehensive security strategy that uses multiple, layered security controls and technologies to protect assets at every level of data center access. With a layered defense in depth approach to security, data center operators and facility managers can protect the data center from the outside in.