- Johnson Controls
- Media Center
- Johnson Controls introduces C•CURE Go Install
Johnson Controls introduces C•CURE Go install app from Software House
MILWAUKEE (January 8, 2017) – Johnson Controls announces the introduction of the C•CURE Go Install app for use with the Software House iSTAR Ultra LT. The new app provides a more efficient, convenient means of configuring or updating information on the iSTAR Ultra LT controller without having to physically access the unit.
Working with an embedded Bluetooth antenna that can be turned on and off remotely to ensure network security, users simply log into the C•CURE Go Install app to perform a host of tasks, including configuring the network settings on the controller, rebooting the device and checking its status. The app is ideal for use with iSTAR Ultra LT controllers that are difficult to access for manual configuration, such as units located high above doorways or behind ceiling tiles.
The password-protected app works for users within range of the controller, including in-house security staff, integrators or installers. Using the app replaces having to make changes on or check status directly from the controller.
“Using the C•CURE Go Install app with the iSTAR Ultra LT minimizes the disruption that can be caused by having to access the controller itself,” said Rick Focke, Director of Product Management, Enterprise Access Control, Building Technologies & Solutions, Johnson Controls. “Increasingly, there are applications, such as hospitals with sealed ceilings, where physical access to the controller just isn’t feasible. Using the intuitive app instead to perform myriad tasks provides a more efficient option.”
For more information on the C•CURE Go Install app for use with the iSTAR Ultra LT, visit http://www.swhouse.com.
About Johnson Controls
Johnson Controls is a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
###
CONTACTS:
Ryan Nolan
Global Public Relations Program Manager
Work + 1 414 524 6170
Mobile +1 414 378 9641
Ryan.P.Nolan@jci.com
Andrea Gural / Chelsie Woods
Eclipse Media Group on behalf of Johnson Controls
+1 207 233 7507 / +1 207 730 2396
agural@eclipsemediagroup.net / cwoods@eclipsemediagroup.net

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)