- Johnson Controls
- Media Center
- VideoEdge TrickleStor technology keeps video surveillance integrity
Johnson Controls’ VideoEdge TrickleStor technology maintains video surveillance system integrity
MILWAUKEE – (April 5, 2018) – Johnson Controls has introduced VideoEdge® TrickleStor, designed to maintain the integrity of video data in a surveillance system in the event of network connectivity loss.
TrickleStor provides a highly-integrated camera and network video recorder (NVR) connectivity solution between VideoEdge NVRs and Illustra® IP cameras that records video locally on Illustra cameras in the event of a connection failure, protecting against video loss in the case of NVR updates or network outage.
When connectivity to the VideoEdge NVR is lost, video is recorded directly onto the camera’s SD card at the same frame rate, resolution and encoding. When connectivity is reestablished, the protected recorded video is automatically inserted into the media database at the correct date and time. The missing video is pulled from the camera to the NVR at an ultra-low bitrate to minimize bandwidth consumption caused by the video retrieval. There is no discernible difference between the trickled-back video and previously recorded video when the stream is reviewed.
When connectivity to the VideoEdge NVR is lost, video is recorded directly onto the camera’s SD card at the same frame rate, resolution and encoding. When connectivity is reestablished, the protected recorded video is automatically inserted into the media database at the correct date and time. The missing video is pulled from the camera to the NVR at an ultra-low bitrate to minimize bandwidth consumption caused by the video retrieval. There is no discernible difference between the trickled-back video and previously recorded video when the stream is reviewed.
For more information on TrickleStor, please visit http://www.americandynamics.net
About Johnson Controls
Johnson Controls is a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
###
CONTACTS:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile +1 414 378 9641
Ryan.P.Nolan@jci.com
Andrea Gural / Chelsie Woods
Eclipse Media Group on behalf of Johnson Controls
+1 207 233 7507 / +1 207 730 2396
agural@eclipsemediagroup.net / cwoods@eclipsemediagroup.net

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)