- Johnson Controls
- Media Center
- Johnson Controls announces new GRINNELL G-Fire One-Bolt Coupling
Johnson Controls announces new GRINNELL G-Fire One-Bolt Coupling
Single-bolt design makes pipe installation faster and easier
MILWAUKEE – (April 16, 2018) – Johnson Controls announces the release of its newGRINNELL G-Fire One-Bolt Coupling with a revolutionary single-bolt design that eliminates alternate tightening and helps contractors perform quicker, more consistent installations with dependable product performance. Other features of the One-Bolt Coupling include:
- Pre-lubricated and pre-assembled for fast and easy push-on installation in both vertical and horizontal applications
- 360-degree contact for an exceptionally rigid joint
- Low-profile spine allows installation of coupling in tighter spaces
- Center-stop gasket ensures proper positioning on pipe
The one-bolt coupling is UL/ULc Listed and FM Approved, with a pressure rating up to 365 psi. It is available in 2-inch to 8-inch sizes (DN50 to DN200) and is available in painted and galvanized finishes.
For more information about the GRINNELL One-Bolt Coupling, visit www.grinnell.com/579. For questions or support, contact technical services at 1-800-381-9312.
About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco® , YORK® , Metasys® , Ruskin® , Titus® , Frick® , PENN® , Sabroe® , Simplex® and Grinnell® . For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
CONTACT:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)