- Johnson Controls
- Media Center
- Illustra Pro line expands with 2MP and 3MP Pro Compact Mini-Domes
Johnson Controls expands Illustra Pro line with 2MP and 3MP Pro Compact Mini-Domes for discrete surveillance
MILWAUKEE - (June 11, 2018) - Johnson Controls is announcing two new camera models to the Illustra Pro line, with the Pro Compact Mini-Domes in 2MP and 3MP resolution, ideal for applications such as retail stores, healthcare facilitiesand banks where low profile and aesthetics are important.
The Illustra 2MP and 3MP Pro Compact Mini-Domes areequipped with various viewing angles including corridor mode,a 9x16 field of view aspect ratio for vertically oriented scenes, which is optimal for hallways, aisles or any area where alandscape format is not ideal.
Rated both IP66 and IP67 for environmental protection as wellas IK10 for vandal resistance, the Pro Compact Mini-Domes can be installed indoors and outdoors for a truly versatile solution.
The Pro Compact Mini-Domes also feature Illustra® IntelliZip compression technology that monitors and adjusts system streaming parameters to match the level of activity in the camera’s field of view. IntelliZip automatically adjusts the video encoder configuration to ensure every detail within the region of interest is captured clearly, minimizing video and storage needs.
Advanced VideoEdge® TrickleStor technology enables edgebased video recording, even in an outage. The camera will automatically detect network interruptions and starts to record video to its SD card followed by a seamlessly video transfer to the NVR’s hard drive once the network connection is reestablished.
For more information visit www.illustracameras.com.
About Johnson Controls
Johnson Controls is a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrolson Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
###
CONTACTS:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile +1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)