- Johnson Controls
- Media Center
- Johnson Controls expands Illustra Pro line with compact mini-domes
Johnson Controls expands Illustra Pro line with 2MP and 3MP Pro compact mini-domes for discrete surveillance
MILWAUKEE (June 11, 2018) – Johnson Controls is announcing two new camera models to the Illustra Pro line, with the Pro Compact Mini-Domes in 2MP and 3MP resolution, ideal for applications such as retail stores, healthcare facilities and banks where low profile and aesthetics are important.
The Illustra 2MP and 3MP Pro Compact Mini-Domes are equipped with various viewing angles including corridor mode, a 9x16 field of view aspect ratio for vertically oriented scenes, which is optimal for hallways, aisles or any area where a landscape format is not ideal.
Rated both IP66 and IP67 for environmental protection as well as IK10 for vandal resistance, the Pro Compact Mini-Domes can be installed indoors and outdoors for a truly versatile solution.
The Pro Compact Mini-Domes also feature Illustra® IntelliZip compression technology that monitors and adjusts system streaming parameters to match the level of activity in the camera’s field of view. IntelliZip automatically adjusts the video encoder configuration to ensure every detail within the region of interest is captured clearly, minimizing video and storage needs.
Advanced VideoEdge® TrickleStor technology enables edgebased video recording, even in an outage. The camera will automatically detect network interruptions and starts to record video to its SD card followed by a seamlessly video transfer to the NVR’s hard drive once the network connection is reestablished.
For more information, visit www.illustracameras.com.
For more information:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions,
Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)