- Johnson Controls
- Media Center
- Launching Tyco DV-5A deluge valve that with new features
Launching Tyco DV-5A Deluge Valve that with New Features
Johnson Controls Launches TYCO® DV-5A deluge valve that offers advanced, streamlined features
Higher pressure rating and lower pressure drop deliver added power and efficiency
(Available in APAC only. Coming soon to Europe and Americas!)
MILWAUKEE – (15 November 2018) – The new TYCO® DV-5A deluge valve from Johnson Controls offers improvements on the DV-5 valve while keeping the original key features valued by customers. The DV-5A deluge valve has a higher pressure rating of up to 300 psi and lower pressure drop, allowing water to travel further at specified system pressure.
The new model features a reduced footprint, thanks to a compact trim package that helps make it easier to install and maintain. The DV-5A also includes an integrated alarm port that eliminates a check valve in pre-action systems.
“We updated the DV-5 to give our customers higher performance and flexibility,” said Gijsbert van Rooijen, global product manager, Johnson Controls. “The enhancements to the new model will boost its overall effectiveness, while making it easier to install, operate and maintain.”
The DV-5A maintains many desirable features of the DV-5, including the single moving part diaphragm design for easier maintenance and operation, as well as an external reset, which reduces the number of steps to bring the valve back in operation after activation. The DV-5A comes with a corrosion-resistant epoxy coating ideal for harsh environments, such as industrial processing plants and outdoor installations. Other features include:
• Easy access to technical information
• Pre-trimmed models available for both deluge and pre-action systems
• Includes next generation BFV-300 butterfly valve with tapping boss (standard in the Americas, available globally)
To learn more about the DV-5A deluge valve, visit www.tyco-fire.com/DV5A. (Available in APAC only. Coming soon to Europe and Americas!)
About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter
# # #
Photo Caption: The new TYCO® DV-5A deluge valve from Johnson Controls offers a higher pressure rating and lower pressure drop, delivering added power and efficiency
CONTACT:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)