- Johnson Controls
- Media Center
- YORK YZ Magnetic Bearing Centrifugal Chiller launches in Middle East
YORK YZ Magnetic Bearing Centrifugal Chiller launches in Middle East
Award-winning chiller offers the widest-operating envelope to support the region’s climate
Johnson Controls is now offering the YORK® YZ Magnetic Bearing Centrifugal Chiller in the Middle East in cooling capacity ranges from 165 to 1350 tons (580 to 4747 kW).
DUBAI – (September 18, 2019) – Johnson Controls is pleased to offer the YORK® YZ Magnetic Bearing Centrifugal Chiller to its Middle East customers. The YORK® YZ delivers up to 35 percent annual energy savings, reduced maintenance costs and is optimized for ultimate performance with a low-GWP refrigerant. Cooling capacity for the Middle East units ranges from 165 to 1350 tons (580 to 4747 kW).
“With the launch of the YORK® YZ chiller, we are proud to be delivering another industry-leading chiller to meet the demands of our customers in the Middle East,” said Claude Allain, VP and GM — Building, Technologies and Solutions, Middle East & Africa. “The extreme, dry climate of the region presents a variety of cooling challenges. Coupled with the success of magnetic bearings in the region, the operating range map of chillers for the Middle East makes the YORK® YZ an ideal choice for a variety of application needs in the Middle East.”
Since its initial launch in 2018 the YORK® YZ has made a significant global impact, capturing top honors in North America, China, Europe, and Australia. The YZ chiller was named 2019 AHR Innovation Award winner in the Cooling category. The success of the chiller has already been seen in the Middle East, as the first YORK® YZ project has been sold in the region. Globally, this is the second largest YZ project sold to date and will be installed later this year.
“With the launch of the YORK® YZ chiller, we are proud to be delivering another industry-leading chiller to meet the demands of our customers in the Middle East.”
— Claude Allain, VP and GM — Building, Technologies and Solutions, Middle East & Africa
The YORK® YZ is the first chiller fully optimized for ultimate performance with a next generation low-global warming potential (GWP) refrigerant – R-1233zd(E). Chosen for its efficiency, safety, availability, low environmental impact and cost, nonflammable R-1233zd(E) has an ultra-low GWP of 1 and is readily available from refrigerant manufacturers.
The YZ chiller can deliver significant energy savings and lower operating costs by taking advantage of the off-design conditions where chillers operate 99 percent of the time. The YZ chiller operates with entering condenser water temperature as low as 40°F (4.5°C), providing enhanced performance in every operating condition and the widest operating envelope in the industry. The YORK® YZ uses an optimized single stage design to provide industry-leading real-world energy efficiency.
The YZ chiller brings together groundbreaking YORK® innovations refined over decades of real-world use to create a revolution in chiller design and optimization. It represents a solution from the chiller experts, who like to think of the YORK® YZ chiller as tomorrow’s chiller, available today.
To learn more about the YORK® YZ Magnetic Bearing Centrifugal Chiller, visit www.YORK.com/Next.
About Johnson Controls
Johnson Controls is a global leader creating a safe, comfortable and sustainable world. Our 105,000 employees create intelligent buildings, efficient energy solutions and integrated infrastructure that work seamlessly together to deliver on the promise of smart cities and communities in 150 countries. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win everywhere, every day and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @johnsoncontrols on Twitter.
# # #
CONTACT:
Sweeney D’costa
Communication & Program Manager
Building Technologies & Solutions, Johnson Controls
Work +971 4309 9941
Mobile +971 564169288
Sweeney.Dcosta@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)