- Johnson Controls
- Media Center
- YORK® YZ Magnetic Bearing Centrifugal Chiller extended to 2,020 tons
YORK® YZ Magnetic Bearing Centrifugal Chiller extended to 2,020 tons
New dual-compressor design with patented heat exchanger technology maximizes chiller performance
The award-winning YORK® YZ Magnetic Bearing Centrifugal Chiller utilizes a new dual-compressor design to expand cooling capacity up to 2,020 tons.
MILWAUKEE – (January 28, 2020) – Johnson Controls is reaching advanced levels of efficiency at even higher capacities with the launch of its expanded YORK® YZ Magnetic Bearing Centrifugal Chiller platform in North America and Latin America markets. Extending the use of magnetic bearings up to 2,020 tons gives more customers the opportunity to experience reduced driveline maintenance and lower operating costs.
Johnson Controls will showcase a model of the extended capacity YORK® YZ Chiller unit at the 2020 AHR Expo (Booth #3833), February 3-5 at the Orange County Convention Center in Orlando.
This expansion in capacity builds on the award-winning YORK® YZ chiller that is optimized around R-1233zd(E) and utilizes an inherent series counterflow design with patented heat exchangers. The extended platform, up to 2,020 tons, is optimized around the environmentally friendly, low GWP refrigerant, providing a future-focused solution today. The YZ chiller design tackles real world energy challenges with the largest operating map in the industry to support the most challenging climates – including the Middle East where the single compressor YZ chiller recently launched.
“With energy efficiency driving customer decisions, we are pleased to offer the extended capacity YORK® YZ chiller to deliver ultimate performance while dramatically reducing cost of ownership.”
— Laura Wand, vice president and general manager, applied equipment, Johnson Controls
“With energy efficiency driving customer decisions, we are pleased to offer the extended capacity YORK® YZ chiller to deliver ultimate performance while dramatically reducing cost of ownership,” said Laura Wand, vice president and general manager, applied equipment, Johnson Controls. “These higher-tonnage systems support the same real-world operating conditions customers have come to expect from YORK, while delivering lower maintenance costs with the use of magnetic bearing technology.”
The advanced, aerodynamic design includes two, single-stage compressors that are paired in a series counterflow arrangement, reducing the lift on each compressor to improve overall full-load and off-design performance. The dual compressor design allows for each compressor to run individually, providing redundancy and improved off-design performance at lower loads. The design also increases turn down capabilities at low loads by continuing to provide cooling on one circuit in the unlikely event of a failure or an unplanned shutdown.
For more information on the YORK® YZ Magnetic Bearing Centrifugal Chiller, visit www.York.com/Next.
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 105,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, York®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)