- Johnson Controls
- Building Insights
- Environmental stability and resiliency where it really matters: your research lab
Environmental stability and resiliency where it really matters: your research lab
Highlights
- Research labs depend on consistent environmental stability to protect the integrity of experiments. Intelligent building automation systems, like Metasys, provide real-time visibility and control to reliably maintain consistent conditions day after day
- Designed specifically for research labs, Metasys critical environments controls solutions continuously measure, analyze and control key environmental variables with precision performance, while Metasys Validated Environments help document, trace and demonstrate compliance in regulated research settings
- Together, these capabilities allow researchers to work with confidence and focus on tomorrow's innovations
Breakthrough research depends on advanced equipment, brilliant minds and an unrelenting desire to advance mankind’s understanding of the universe. But it also depends on precise control of multiple environmental variables within a research lab. Sensitive research materials and equipment require continuous control of environmental variables within tight tolerances, no matter the conditions outside the lab. Because in environments like electron microscopy suites, biosafety labs, and cleanrooms, science only holds up when the environment does.
Universities and colleges that can deliver the required level of research lab environmental stability accelerate discovery, strengthen experiment repeatability and position themselves as more reliable partners for public and private enterprise collaboration. This sets a powerful research flywheel in motion. When labs maintain stable conditions, researchers deliver credible results. Those results draw new partners and funding, which help expand facilities and capabilities, accelerating discoverability and results over time.
And it starts with getting the lab environment right, consistently and reliably, every day.
What it takes to maintain stability in advanced research environments
On campus, research labs rarely operate in isolation. On most campuses, they coexist with faculty spaces, classrooms, legacy buildings and infrastructure built decades apart. At the same time, today’s research protocols demand tighter tolerances, higher air change rates, stricter pressure relationships and robust documentation aligned to standards such as ANSI, ASHRAE and ISO. Maintaining environmental stability in this context isn’t about managing a single variable; it’s about coordinating many systems, continuously, under changing conditions.
As James Rosner, higher education expert at Johnson Controls, explains: “Maintaining indoor air quality, precise temperature control and humidity is critical for achieving breakthroughs. When these environmental elements are stable, researchers can focus on what really matters – the discoveries that help advance society. When they’re not stable, even small fluctuations can lead to major impacts. Samples and data, can be lost forever, which can set research back several years.”
This level of control requires more than basic building automation. Research labs require real-time monitoring, trend logs, predictive analytics and intelligent systems automation purpose-built to maintain environmental stability and resiliency.
At Johnson Controls, precision control is not only in our name, it's in our DNA. The company was founded when Warren Johnson invented the first electric room thermostat to keep his classroom at a comfortable temperature. That need for stable environments has only grown over time, especially in mission-critical environments like research labs that rely on smart controls, advanced automation and systems that adapt to changing conditions.
Together, they maintain precise environmental conditions where research outcomes depend on it most. Achieving this level of precision requires continuous measurement and control of airflow, indoor air quality, temperature, pressure and humidity. Advanced building automation systems like Metasys make it possible to measure and control these variables, providing the best environment for cutting-edge research.
Labs controlled with a higher degree of confidence
“Laboratories are some of the most difficult places to control.”
Bernard Clement, HVAC & Controls expert at Johnson Controls
Building controls like Metasys drive environmental stability and resiliency in research labs by serving as the central intelligence that coordinates HVAC systems to maintain precise conditions. Through continuous monitoring, predictive analytics and quick reaction to changing conditions, Metasys enables enhanced uptime, resiliency and compliance with multi-server redundancy and rapid recovery to safeguard research that may have been running for months, or even years.
The Metasys Critical Environment Equipment Controller is an integral part of Johnson Controls Critical Environments solutions suite. This controller is specifically designed for research labs to provide rapid and accurate response to changing conditions, with 3.75 times faster PID loops and 10 times faster analog input refreshes than average. This performance is especially important for seemingly simple events that have a significant impact in lab environments, such as door openings and fume hood sash movements. The Metasys Critical Environment Equipment controller helps maintain the precise environmental conditions that enable cutting-edge research to progress uninterrupted.
Beyond precision performance, Metasys Critical Environment Controls ensure research labs meet stringent ventilation and safety requirements. These requirements include sterile environment controls (USP 797), specialized ventilation and pressurization (ANSI/ASHRAE/ASHE), and handling of hazardous compounds (USP 800).
Metasys Validated Environments complements critical environment controls by supporting data integrity and traceability, helping research facilities document and demonstrate compliance. Metasys therefore not only reinforces confidence in research integrity, but also in regulatory compliance.
Commercial HVAC represents the muscles that execute precision performance, but Metasys BAS is the brain that orchestrates the right equipment. While mechanical equipment delivers airflow and temperature control, Metasys constantly interprets environmental data, anticipates possible changes and guides systems with the intelligence and speed required in mission-critical laboratories.
Final insight
Ensuring uptime, maintaining precision performance and protecting research integrity is a complex task – but it’s not impossible, especially with the right technology partner. Whether you’re starting a new project or retrofitting a historic facility, Johnson Controls can keep you ahead of the curve.
Unlock precision performance for your research lab
FAQs
How much money can a college or university save with Johnson Controls?
With the right system, it’s possible to save up to 30% on energy costs. One leading Georgia university was able to cut $90k in costs with data-driven maintenance.
Can Johnson Controls help my college or university meet its decarbonization goals?
Absolutely. For example, we helped Stanford reduce peak energy demand by 17% and lower GHG emissions by 68%.
Can Johnson Controls help my college or university integrate alternative energy sources?
Yes. As proof, we partnered with Southwestern Oregon Community College (SWOCC) to deliver $11M of infrastructure upgrades, including the installation of solar technology to help reach their sustainability goals. They also expect to reduce utility spending by at least 35% and save more than $17 million in energy costs over the project’s lifespan.
Is Metasys compatible with 3rd party equipment?
Yes. Metasys is built on an open architecture that is designed to be interoperable with a wide range of third-party building systems and devices. It supports widely used protocols, including BACnet, Modus, LonWorks, KNX, etc., letting universities manage HVAC, lighting, fire, security and other building systems from a single interface.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)