10 min read
October 06, 2026

Share

Highlights

  • Predictive maintenance requires a phased approach with each stage paving the way for the next stage
  • The predictive maintenance process includes auditing assets, integrating data sources, deploying analytics and connecting CMMS workflows
  • A well-configured predictive maintenance strategy can have a profound effect on an organization by reducing unplanned downtime, lowering energy costs and improving equipment lifespan

Predictive maintenance has become a priority for facilities and operations leaders looking to reduce downtime, control costs and improve equipment reliability. Traditional maintenance approaches often leave organizations reacting to failures or servicing equipment based on schedules rather than actual need.

Predictive maintenance changes this approach. By combining operating data, historical performance information and analytics, organizations can identify potential issues early and act before equipment failures disrupt operations.

Building a successful predictive maintenance program requires more than technology alone. It requires a clear strategy that aligns people, processes and systems. This guide outlines a phased approach for developing a strategy across commercial buildings and portfolios, so organizations can plan in advance, maximizing uptime and extending equipment life.

Learn why predictive maintenance is critical for optimizing equipment performance

Learn more

How to Build a Predictive Maintenance Strategy: A Phased Approach

Building a predictive maintenance strategy is a phased process where each step lays the foundation for the next. Skipping ahead or managing steps out of order risks leaving gaps that can be difficult or expensive to fix later.

This section provides a detailed roadmap to get you to fully operational predictive maintenance.

Phase 1: Audit Your Assets and Current State

A predictive maintenance rollout starts with an honest assessment of your current environment and any barriers to success. Not all assets in a building require a predictive maintenance approach, so start by prioritizing those that pose the highest risk if they fail.

Chillers are a good example. A chiller failure in a critical environment like a hospital puts patient health at risk, so predicting issues and avoiding failures altogether is a priority. By comparison, a unit heater in an underused storage room isn’t as critical and would be just fine on a calendar-based preventive approach.

Alongside prioritizing equipment, organizations should assess their current data, systems and maintenance processes. Assess what data your Building Automation System (BAS) is already capturing, examine current workflows and understand how well your Computerized Maintenance Management System (CMMS) is adopted across teams.

Matching the right approach to the right equipment is the first strategic decision to make. It also sets the foundation for the following phases.

Phase 2: Establish Condition Baselines and Integrate Data Sources

The next step is building a strong data foundation. Predictive analytics tools require sufficient historical and real-time data to understand what normal equipment performance looks like and recognize when conditions begin to change.

Much of this data already exists, but it's often siloed. This can make it difficult to create a predictive maintenance workflow. Research on building system integration shows data fragmentation between BAS systems, IoT sensors and CMMS platforms is one of the main barriers to predictive maintenance.

The challenge becomes even greater as portfolios expand, and data volumes increase. Companies with large, distributed portfolios can face challenges in being able to rationalize the data coming from buildings in a way that makes sense. These data sources must be properly integrated so that data flows seamlessly from sensors to analytics and on to work orders.

Phase 3: Deploy Analytics and Fault Detection

The analytics tools continuously monitor real-time equipment data and compare it against baselines. But unlike condition-based maintenance - which triggers an alert once a threshold has been crossed - predictive analytics tracks data trajectories over time. It can highlight performance trends that may indicate future failures before they become operational issues.

Fault Detection and Diagnostics (FDD) tools complement this analysis by identifying and diagnosing specific fault patterns. This can help teams understand what might be causing the issue.

Early warning signs allow teams to plan maintenance in advance, avoiding failures and unexpected downtime. Analytics tools help facilities teams focus on the most important signals by identifying patterns that may otherwise go unnoticed.

Phase 4: Define Response Workflows and Connect to CMMS

A fully integrated CMMS takes analytics insights and turns them into prioritized work orders with clear escalation paths. This means technicians can arrive at the equipment fully briefed on the relevant data and the perceived fault, and can get to work straight away. When systems are fully integrated, many of these workflows can be automated. This can help reduce manual effort and accelerate response times.

As highlighted in Phase 2, data integration makes the end-to-end workflow possible. Without it, predictive maintenance can't be fully automated or deliver its full value.

Phase 5: Measure, Refine and Scale

Once you’ve completed the first four phases, the focus shifts to evaluating whether the strategy is working and building a case to roll it out. Ideally, this will take the form of an early 90-day review followed by quarterly or semi-annual reviews, depending on the organization's capacity.

The asset history generated in Phase 4 is crucial for this stage. Reviewing repair frequency and fault patterns helps determine whether issues are being identified early enough and whether teams are focused on the right signals. This stage is also an opportunity to review and refine. For example, you may need to adjust baselines for certain equipment to ensure the right signals are flagged and acted upon.

Once stakeholders are satisfied with performance across priority assets, the same strategy can be rolled out to other equipment and sites.

Watch our webinar on building a roadmap to predictive success

Watch now

Building the Business Case for Predictive Maintenance

Predictive maintenance requires considerable upfront investment. Beyond maintenance savings, predictive maintenance helps reduce operational risk and gives organizations greater confidence in capital planning decisions.

Building owners and operations leaders need to be able to justify the initial cost and effort involved to stakeholders around the business, with an ability to focus on critical metrics including:

  • Maintenance labor efficiency
  • Reduction in unplanned downtime
  • Emergency repair costs
  • Energy consumption
  • Asset uptime

When doing so, it’s important to remember the cost of doing nothing. Reactive and preventive maintenance approaches carry risks which can echo across the business. Reactive maintenance bills can run up quickly with emergency callouts and unplanned downtime, whereas preventive maintenance risks servicing equipment that doesn’t need it. This can mean wasting money and still missing issues that occur between checks.

Instead of scrambling to deal with the unexpected, predictive maintenance helps teams plan for problems instead of reacting to them.

Cost Avoidance vs. Maintenance Spend

Predictive maintenance requires upfront investment in technology and infrastructure, but it shifts spending from reactive to strategic. The cost of emergency repairs and unplanned downtime add up fast. Catching a fault early and paying for a minor repair is far cheaper than replacing an entire piece of equipment out of hours because it shut down unexpectedly.

Over time, many organizations justify the investment through reduced downtime, fewer emergency repairs and improved operational efficiency.

Asset Life and Capital Planning

Equipment that runs within “normal” parameters lasts longer. Chillers have a median lifecycle of 20-23 years, according to the American Society of Heating, Refrigerating and Air-Conditioning Engineers (ASHRAE). However, that figure depends on whether equipment is properly maintained and operated within normal parameters. By catching issues before they become problems, predictive maintenance helps to extend the equipment lifespan and save money in the long run.

Predictive maintenance can help organizations better understand an asset's remaining useful life (RUL) and identify opportunities to maximize it through proactive intervention. Rather than planning to replace equipment after a set period, this strategy provides accurate assessments and indicates when investment will be needed.

Energy Efficiency: An Often-Overlooked Benefit

HVAC systems run continuously and are among the heaviest energy consumers in a commercial building - chillers alone can account for up to 40% of a building's total energy costs.

When those systems run outside the expected parameters, they drain energy unnecessarily. Predictive maintenance catches performance drift early to identify potential issues before they lead to increased energy use, additional cost, or unnecessary equipment failure.

Predictive Maintenance Strategy Across Multi-Site and Enterprise Portfolios

Scaling predictive maintenance strategy beyond a single building makes integration even more crucial. Siloed systems make it difficult for teams to compare performance across sites. As noted in Johnson Controls 2026 building predictions, the value of connected buildings will depend on how seamlessly ecosystems communicate.

That seamlessness allows a single view across different sites to reduce visibility gaps and allow organizations to compare equipment performance data.

Standardizing Workflows Across Facilities

It’s not enough to connect everything from a technical standpoint. Standardized workflow, naming conventions and operating thresholds help ensure performance comparisons remain meaningful across facilities.

This involves a consistent asset naming structure and baseline thresholds, with protocols in place should something be flagged. Otherwise, the strategy and insights differ considerably between facilities.

Centralized Reporting and Performance Benchmarking

A portfolio-level strategy means organizations can enjoy cross-site visibility and compare performance between buildings. This means they can make better-informed decisions and act on patterns that they wouldn’t spot with a single-site view.

This data also feeds into capital planning, meaning resources can be allocated to where they’re most needed rather than in order of request.

Once you start operating at portfolio level, predictive maintenance becomes a vital business intelligence tool.

Common Pitfalls That Undermine Predictive Maintenance Strategy

Adopting predictive maintenance is a multi-step process, and there are many elements to get right. Here are some of the common oversights facilities teams make during implementation:

  • Starting with technology instead of strategy: Define priorities and workflows before investing in tools
  • Poor data quality and integration gaps: Incomplete or inconsistent data leads to unreliable insights
  • Neglecting the human side: Teams need training, clear workflows and ownership

Start Building a Smarter Predictive Maintenance Strategy

A predictive maintenance strategy involves a significant shift in operations, with benefits that can be felt beyond the facilities team. To get the most out of the technology, teams must build a smart, robust strategy to ensure seamless implementation within an organization.

Ultimately, predictive maintenance is not just about avoiding equipment failures. It is about creating more predictable building operations and making better-informed business decisions.

Learn how Johnson Controls helps facilities and operations teams build predictive maintenance strategies.

Predict problems. Minimize downtime.

Connect with an expert

FAQs

1. What is a predictive maintenance strategy?

A predictive maintenance strategy involves planning how the approach will work in practice. It involves setting a clear implementation roadmap that addresses core issues such as auditing assets, integrating data sources, deploying analytics and connecting CMMS workflows.

An effective strategy uses real-time sensor data and advanced analytics tools to identify emerging equipment issues before they contribute to failures, downtime or increased operating costs.

2. What are the biggest barriers to predictive maintenance adoption?

Data quality and integration are among the most common barriers to predictive maintenance adoption. Incomplete, inconsistent or disconnected data can reduce confidence in predictive insights, while poor integration prevents information from moving efficiently between systems. Organizations also need stakeholder buy-in, clear ownership and well-defined workflows to support long-term success.

3. What data do you need for predictive maintenance?

The foundation data required for predictive maintenance comes from Building Automation Systems (BAS) data, Internet of Things (IoT) sensors and historical records. This data will likely already be in place; to be useful for predictive maintenance, it has to be structured consistently across assets and sites. That way, it can support meaningful predictive analytics and maintenance decision-making.