- Johnson Controls
- Customer Success Stories
- Ansul Restaurant Systems
Custom Fire Protection Solutions Deliver Significant Economic and Operational Benefits
Delivering compliant, reliable fire protection in a high-demand commercial kitchen
A major hotel in Scotland identified a critical fire safety gap within its main kitchen. Working with FireRite, an authorised ANSUL distributor, the hotel implemented the ANSUL® R-102 Restaurant Fire Suppression System - enhancing safety for staff and guests while meeting insurance and regulatory requirements.
Impact Highlights
Enhanced fire safety for staff, guests and valuable hotel assets
Full compliance with insurance and EN standards, supporting risk mitigation
Future-ready protection with a flexible system designed for evolving kitchen layouts
Addressing Fire Risk in High-Throughput Commercial Kitchens
Commercial kitchens present a heightened fire risk due to the constant use of cooking appliances, particularly those involving fats, oils and grease. At this hotel, the absence of an existing fire suppression system in the main kitchen created a significant safety and compliance gap.
Cooking equipment is a leading cause of workplace fires in the UK, making reliable protection essential in hospitality environments. At the same time, any disruption to kitchen operations could directly impact customer service and business continuity.
The hotel required a solution that would:
- Meet strict insurance and regulatory requirements
- Provide reliable protection against grease-related fire risks
- Adapt to potential future changes in kitchen layout
- Minimise disruption during installation and operation
A Flexible, Compliant Fire Suppression System for Commercial Kitchens
FireRite worked closely with the hotel to design and deliver a tailored solution based on the ANSUL® R-102 Restaurant Fire Suppression System.
Following a structured design process - including remote assessments and on-site verification - the team selected the ANSUL R-102 system for its proven performance, industry reputation and compliance credentials.
Key elements of the solution included:
- EN 17446-compliant system design providing assurance for insurers and stakeholders
- Overlapping nozzle coverage to ensure continuous protection, even if kitchen equipment is reconfigured
- Scalable, adaptable system layout to support future operational changes
Installation was completed in a single day by FireRite’s trained technicians, minimising disruption to hotel operations. Following commissioning, staff received comprehensive training covering system operation, emergency activation and maintenance best practices.
“The brand recognition is a major driving factor in simplifying sales… Our team truly values the market-leading technical support they provide. It’s always there for us and just makes the whole process easier.”
John Jepson, FireRite
Improved Safety, Compliance and Peace of Mind
The ANSUL R-102 system delivered a robust, future-ready fire suppression solution tailored to the hotel’s requirements. The kitchen is now protected by a reliable system designed to respond quickly to grease fires while supporting safe, continuous operations.
With full regulatory compliance achieved and insurer expectations met, the hotel has strengthened its overall risk management strategy. The flexible system design ensures ongoing protection, even as kitchen layouts evolve over time.
The project highlights the value of combining trusted ANSUL technology with FireRite’s technical expertise - resulting in a high-quality installation that enhances safety, reliability and operational confidence.
About the facility
- Major hotel in Scotland with a high-throughput commercial kitchen environment
- Critical food service operations requiring continuous uptime and safety compliance
- Grease-intensive cooking environment with elevated fire risk from oils and cooking appliances
Solutions:
Similar stories
San Francisco International Airport strengthens fire protection and operational continuity with advanced foam suppression system
SFO partnered with Johnson Controls to implement a high-performance, non-fluorinated foam suppression system that delivers fast, reliable fire protection while supporting long-term operational resilience.
Protecting over 600,000 artifacts at Mexico City’s National Museum of Anthropology
Advanced fire detection and clean-agent suppression systems safeguard one of Latin America’s most important cultural collections while supporting safety and compliance.
Custom Fire Protection Solutions Deliver Significant Economic and Operational Benefits
Johnson Controls partners with a global retailer to upgrade fire protection systems across thousands of stores with minimal operational disruption
Las Vegas resort saves $110k annually with OpenBlue
Discover how a Las Vegas mega resort cut energy use by 10.2% and saved $110K annually using Johnson Controls OpenBlue Central Utility Plant Optimization.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)