- Johnson Controls
- Customer Success Stories
- Cache County School District
Cache County School District modernizes facilities through guaranteed savings
Funding infrastructure improvements through a self-funding performance contract
Cache County School District wanted to conserve energy, reduce costs and address facility needs across its 24 schools but lacked the resources to develop and manage a large-scale modernization effort. Working with Johnson Controls, the district implemented a self-funding performance contract that supports facility improvements through guaranteed energy and operational savings.
Impact Highlights
$16M+ guaranteed savings over 20 years
$750K+ in grants and rebates secured
12M+ kWh electrical avoidance
Limited resources constrained facility modernization effort
Expanding the scope of facility improvements through performance contracting
Johnson Controls conducted a comprehensive facility audit to identify opportunities that extended beyond traditional energy-saving measures. Following the assessment, Cache County School District implemented a self-funding performance contract designed to support facility improvements through guaranteed energy and operational savings.
The project included district-wide LED lighting and lighting controls, new and upgraded Metasys Building Automation Systems, building envelope improvements, upgraded fire and carbon monoxide alarm systems, air conditioning for two high school auditoriums, plug load control and electrical power factor correction, swimming pool operational improvements and new 485.5kW photovoltaic solar systems. The initiative also supported classroom improvements at older facilities while helping address deferred maintenance needs across the district.
“It was a great experience for us to see how many ways it was possible to improve efficiency and provide a better learning environment for what was, essentially, a cost neutral position."
Dale Hansen
Business Administrator, Cache County School District
Transforming school facilities through guaranteed performance
The self-funding performance contract supports infrastructure modernization across 24 schools and is guaranteed to generate more than $16 million in energy and operational savings over 20 years. The project has also helped the district secure more than $750,000 in grants and rebates, creating additional financial value while supporting long-term facility improvements.
The modernization initiative is expected to help create more comfortable, safe and effective learning environments while addressing deferred maintenance needs and improving facility consistency across the district. Energy-saving measures and system upgrades are projected to deliver:
- More than $16 million in guaranteed energy and operational savings over 20 years
- More than 12 million kWh of electrical avoidance
- More than 4,500 kW of demand avoidance
- More than 250,000 therms of natural gas avoidance
- More than 10,000 metric tons of CO₂ avoidance equivalent to over 1 million gallons of gasoline consumed
While implementation was still underway at the time of the case study, district leaders reported early operational improvements, including significantly improved electrical power factor performance.
About Cache County School District
About the facility
- Serves 18,000+ students across 24 schools
- Located in northern Utah, United States
Solutions:
Similar stories
American curriculum school in UAE projects 13% energy savings
A K–12 school uses digital building insights to identify nearly 13% energy-saving potential and cost-avoidance opportunities.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)