- Johnson Controls
- Customer Success Stories
- Northern China hospital improves operational visibility across specialist buildings
Northern China hospital improves operational visibility across seven specialist buildings
Integrated building management systems supports complex clinical environments across a large hospital campus
Impact Highlights
4,600+ BMS control points managed campus-wide
One platform across seven specialist buildings
Faster, more coordinated operational responses
Coordinating multiple systems across specialist buildings and clinical zones
The hospital needed to manage complex control requirements across seven specialist buildings and multiple clinical zones. Its building management system covered more than 4,600 control points across a campus of more than 214,000 square meters, creating a broad operational environment for facility teams to oversee.
The hospital also needed to bring HVAC, energy, lighting, air quality and medical support systems into one building management system. The approach had to maintain reliable and manageable operation across a large number of control points while supporting the distinct requirements of functional areas within the campus.
To improve operational efficiency, the facility required clearer visibility across buildings and systems. It also needed an approach that could help teams respond in a faster, more coordinated way while supporting ongoing energy performance and long-term sustainability.
Zone-based control and multi-system integration on one platform
The hospital deployed the EasyIO Neo Series to provide scalable, zone-based building control across the campus. The seven specialist buildings were divided into functional zones, helping operations teams simplify day-to-day operation and maintenance while addressing the control requirements of different clinical areas.
EasyIO 8000 controllers support distributed control and third-party integration. The deployment included 173 CW IP controllers and 212 IO modules, supporting 4,631 control points across the facility. This distributed approach enabled control to be organized around the hospital’s functional zones rather than managed as a single undifferentiated environment.
Through multi-system integration, the hospital unified HVAC, lighting, energy, air quality and medical support systems on one platform. The integrated approach gives facility teams a clearer view of performance across systems and buildings while retaining zone-level control.
Johnson Controls supported the hospital’s objective of creating a building management approach that could operate across a large, complex healthcare campus. The resulting platform brings the facility’s core building and support systems together while keeping operation and maintenance organized around the needs of each functional zone.
Better visibility supports coordinated responses and ongoing optimization
The integrated platform now supports more than 4,600 building management system control points across seven specialist buildings and more than 214,000 square meters. By bringing multiple systems together, the hospital simplified building management across the campus.
Improved operational visibility enables faster, more coordinated responses. Facility teams can view HVAC, lighting, energy, air quality and medical support systems through one platform, while the functional-zone structure supports manageable operation and maintenance across the hospital’s specialist buildings and clinical areas.
Zone-level energy data supports ongoing performance optimization, improved equipment efficiency, system reliability and operational performance. The integrated approach supports improved energy performance and enhances operations and sustainability across the campus. Together, these outcomes support more consistent healthcare operations and the hospital’s long-term sustainability objectives.
About the Customer
About the facility
- One of the largest hospitals in Shaanxi Province, northern China
- Seven specialist buildings spanning more than 214,000 square meters
- More than 4,600 building management system control points
Solutions:
Similar stories
Children’s of Alabama cuts natural gas use by 69%
Partnering with Johnson Controls, Children’s of Alabama is advancing efficiency and sustainability through smart infrastructure upgrades that enhance patient care while lowering operating costs.
Cortellucci Vaughan Hospital improves efficiency & sustainability
Cortellucci Vaughan Hospital, Canada’s first smart hospital, uses OpenBlue and Metasys to reduce energy use, improve operational performance, and enhance patient experience, earning LEED Silver certification and ranking among top performers in energy efficiency.
Jupiter Hospital achieves up to 500 kWh in daily energy savings
Jupiter Hospital automated chiller plant operations with Johnson Controls and Graylinx, improving efficiency with the Chiller Plant Optimizer.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)