- Johnson Controls
- Building Insights
- How to implement predictive maintenance analytics
Predictive maintenance analytics: how better insight leads to smarter maintenance
Highlights
- Predictive maintenance analytics processes large volumes of data from across building systems to learn what normal equipment operation looks like
- When performance begins to shift, predictive maintenance analytics flag early warning signs to help facility teams identify potential problems before they escalate into equipment failures or costly downtime
- For predictive maintenance analytics to deliver meaningful value, organizations must be data-ready
- Being data-ready means having high-quality data sources, standardized asset information and integrated systems that allow analytics to operate reliably at scale
Unexpected equipment failures rarely happen without warning. The challenge is that many facility teams lack the tools to spot those warnings early enough to act. Predictive maintenance analytics helps organizations spot developing equipment issues before they lead to downtime, comfort complaints or unnecessary energy costs.
Predictive maintenance analytics goes beyond traditional predictive maintenance by layering AI, machine learning (ML) and IoT (Internet of Things) sensors onto condition-based monitoring. It turns data into intelligent forecasts to help facilities teams anticipate faults or asset decline before they occur.
Predictive maintenance, as a broader strategy, prioritizes maintenance decisions based on asset condition rather than on a fixed schedule (preventive) or on when a machine breaks down (reactive). It allows facilities teams to adopt a more proactive, data-driven strategy that cuts downtime and helps assets continue working for longer.
Predictive maintenance has matured significantly with AI and ML. What we now call predictive maintenance analytics represents that more sophisticated tier.
Without AI-driven analytics, predictive maintenance is still condition-based and data-driven. It relies on a mixture of manual data analysis and rule-based fault detection, rather than intelligent “thinking.” The AI layer improves accuracy, scale and automation.
This article will explain how predictive maintenance analytics helps you make risk-based decisions and assess your organization’s data readiness to adopt it. For facility leaders, the result is fewer unexpected equipment failures, improved energy performance, reduced maintenance costs and greater confidence in capital planning.
Learn more about our predictive and diagnostic services
How predictive maintenance analytics works
Modern BAS platforms serve as a critical foundation for predictive maintenance analytics because they collect and centralize operational data from connected equipment throughout the building.
Predictive maintenance analytics takes data from multiple building systems and translates it into helpful insights for facilities teams. It learns normal operating ranges for each asset and establishes performance benchmarks to make it easier to detect early signs of decline.
When issues do arise, it can interpret the data to make specific maintenance recommendations.
Johnson Controls combines building automation, connected equipment, service expertise and AI-driven analytics into a single ecosystem. Unlike approaches that evaluate individual assets in isolation, Johnson Controls helps organizations analyze and optimize performance across entire buildings and portfolios. This provides a more complete view of operational risk and opportunity.
Data collection and integration
Predictive maintenance analytics relies on data from many existing sources that include Building Automation Systems (BAS), IoT sensors, runtime meters and equipment telemetry. Together, they create a comprehensive view of building operations across individual assets, sites and portfolios.
With so much data being recorded, quality is essential. If data is inconsistent or missing information, it directly impacts the reliability and effectiveness of the system. Platforms such as Metasys help aggregate equipment and building performance data to create a foundation for advanced analytics and maintenance insights.
Baseline modeling and anomaly detection
Predictive maintenance analytics establishes a baseline of normal equipment behavior. By understanding typical operating conditions, the system can identify unusual performance patterns that may indicate developing issues.
If incoming data falls outside the expected range, facility teams can assess whether a potential failure or fault has occurred.
Forecasting failure risk
Predictive maintenance analytics projects how equipment performance will change over time, estimating both performance decline and failure risk. It uses historical performance and operating data to estimate when intervention may be needed.
Interpolation calculates and fills in unknown values that fall between two known data points. If your energy meter stops reporting for a few hours due to a network issue, the Metasys Energy Dashboard looks at the reading right before the gap and the reading immediately following the gap. It presumes the energy was consumed at a steady rate and creates a line between these two points to estimate the missing value.
Extrapolation estimates unknown values that fall outside the range of an available data set. For instance, if you have available data until Tuesday but need to estimate usage until Thursday, the system reviews historical consumption trends and extends the current trend line forward to predict the missing data.
Translating insights into maintenance action
Analytics must connect to operational workflows to be truly valuable. A closed-loop system uses insights to trigger prioritized and documented work orders. This can be automated or handled manually through a maintenance platform integration, such as a CMMS, and should include a high level of asset information to inform the technician.
Remember, predictive maintenance analytics can only improve asset reliability if insights are translated into action.
Analytical techniques used in predictive maintenance analytics
Predictive maintenance analytics relies on multiple modeling and statistical techniques to identify patterns in asset performance degradation, anticipate future faults and prioritize maintenance efforts.
Here are some of the techniques used in predictive maintenance analytics:
- Trend analysis: Looks at historical data to detect a gradual decline in efficiency or asset drift. Small changes that aren’t big enough to trigger an alarm can still identify issues over time.
- Statistical process control (SPC): Uses control limits to understand what “normal” looks like. When performance deviates outside of those parameters, it flags the issue before a failure occurs.
- Time-series forecasting: Uses time-dependent models to project future faults from existing data and predict when systems may exceed thresholds.
- Signal processing: Analyzes sensor signals from motors, pumps and fans to identify potential issues.
- Machine learning models: Identify patterns and correlations across data sets that aren’t immediately obvious. These models can be refined and improved over time as more data becomes available.
- Fault detection and diagnostics (FDD): Uses rules or models to detect anomalies and faults. It then works to identify what may be causing the issue.
- Regression-based modeling: This examines how one variable changes in relation to others (such as energy consumption versus temperature), which helps establish what normal performance looks like and highlights if behavior starts to shift.
Applying predictive maintenance analytics in commercial HVAC systems
The above techniques combine to help identify several common HVAC system issues,, show what’s happening and inform what is likely to happen next.
For example, predictive maintenance analytics may detect gradual chiller efficiency drift before facility staff notice a problem. This allows maintenance teams to investigate and resolve the issue before higher energy costs, comfort complaints or equipment failure occur.
While HVAC is a common application, similar techniques can be applied to electrical systems and other critical building infrastructure.
How predictive maintenance analytics can strengthen risk-based decision-making
Predictive maintenance analytics is excellent at helping facilities teams identify the risk of asset failure and plan for it effectively.
With AI-driven analytics helping to spot chiller faults up to 48 hours and with 82% accuracy, service experts can validate insights and coordinate a response. This helps them move from a reactive “break-fix” style of maintenance to a more risk-based one, prioritizing assets by criticality and failure probability before problems escalate.
AI and predictive diagnostic technology allow for better performance, efficiency and reliability of assets.
Is your facility ready for predictive maintenance analytics?
Before investing in predictive maintenance analytics, facilities leaders should assess whether their organization is ready. Consider the following questions before making the decision:
- Do we have enough sensor coverage across all critical assets?
- Is our historical performance data reliable enough to establish meaningful baselines?
- Are asset hierarchies and data streams standardized for analysis?
- Do our teams have the processes and knowledge to interpret analytics and act on recommendations?
- Are maintenance workflows ready to integrate insights from predictive models?
If the answer to any of these questions is no, address those gaps through a phased roadmap before making significant analytics investments. Not all gaps carry equal weight. Incomplete sensor coverage can be addressed incrementally as the system scales, but data quality and standardization issues need to be resolved up front. Without real-time data, predictive analytics are limited.
Predictive maintenance analytics transforms raw building data into foresight. This provides teams with the intelligence to make proactive, risk-informed maintenance decisions.
Ready for data-driven asset performance?
FAQs
-
What are the KPIs for predictive maintenance?
There are multiple ways to measure success in predictive maintenance. These include mean time between failures (MTBF), mean time to repair (MTTR), maintenance cost per unit and planned maintenance percentage (PMP). How you measure success will depend on your organization’s overall goals.
-
What is PM vs PdM?
Preventive maintenance (PM) is proactive, scheduled maintenance based around either time (every six months) or usage (every 10,000 run hours). It involves routine inspections designed to catch issues before they occur and avoid expensive emergency repair costs or unplanned downtime.
By comparison, predictive maintenance (PdM) uses sensors to respond to the actual condition of each asset. It offers a personalized approach to maintenance based on an asset's health over time. On the other hand, preventive maintenance risks over-servicing or under-servicing because of its reliance on a set schedule.
-
Which type of data is most commonly used in predictive maintenance analytics?
The most used data is time-series data taken from IoT sensors and building systems. This is because this data is continuous and allows predictive maintenance analytics to track performance over time from a range of signals.
However, it is best used alongside other data types – including asset metadata and maintenance history – to build up a comprehensive picture.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)