- Johnson Controls
- Customer Success Stories
- Major Cold Storage Facility
Ensuring always-on cold chain operations in Singapore
Modernizing a major cold storage facility to support national food security in Singapore
Impact Highlights
Maintained continuos operations during the retrofit
Reduced risk of disruption to critical operations
Lower environmental impact with zero-GWP refrigerant
Replacing ageing refrigeration infrastructure without disrupting critical operations
The facility had relied on a single, centralized refrigeration system for more than 25 years. Ageing equipment, declining insulation performance, and the absence of system redundanc posed significant operational risks. A single failure could disrupt the entire cold chain.
At the same time, the facility operates around the clock and plays a critical role in Singapore’s food supply, in a country where more than 90% of food is imported. Any downtime would have direct implications for food availability and safety.
The challenge was further compounded by evolving regulatory requirements. In line with Singapore’s Green Plan 2030, the facility needed to transition away from hydrofluorocarbon (HFC)-based systems toward more sustainable, low-impact alternatives, without interrupting day-to-day operations.
A phased, always-on refrigeration upgrade designed for resilience and sustainability
The facility partnered with Johnson Controls to deliver an end-to-end refrigeration upgrade, replacing legacy systems while maintaining continuous operations.
The upgrade was executed through a carefully planned, five-year phased approach. Precision sequencing allowed individual systems to be replaced incrementally, aligned with cold room usage cycles, ensuring uninterrupted service throughout the transformation.
As part of the solution, the facility transitioned from HFC-based refrigerants to ammonia, selected for its high efficiency and zero ozone depletion and global warming potential. Safety and resilience were enhanced through built-in redundancies, ammonia detection alarms, and real-time monitoring systems.
This approach enabled the facility to move from a single-point legacy system to a more robust, future-ready refrigeration infrastructure.
A resilient, sustainable cold chain built for continuous operation and national food security
Through a carefully phased retrofit, the facility replaced its ageing refrigeration infrastructure without disrupting round-the-clock operations. This transfomration strengthened resilience, improving safety, and aligned the facility with Singapore’s long-term sustainability and food security objectives.
Key outcomes include:
- 24/7 continuous operations maintained throughout a complex, five-year retrofit program, avoiding disruption to critical cold chain activities.
- More than 300 individual cold rooms supported by upgraded, modern refrigeration infrastructure.
- Reduced operational risk by eliminating reliance on a single, ageing refrigeration system and introducing built-in redundancy.
- Improved safety and operational visibility through ammonia detection alarms and real-time monitoring systems.
- Lower environmental impact with zero-GWP, zero-ODP refrigerant.
- Alignment with national sustainability goals, supporting Singapore’s Green Plan 2030, Green Mark standards, and long-term food resilience objectives.
As a result, the facility now operates as one of Singapore’s most advanced cold chain hubs, with infrastructure designed to support future demand while contributing to national food security and sustainability goals.
About the Major Cold Storage Facility
About the facility
- One of Singapore’s largest, most advanced cold chain hubs
- Critical to national food security in an import-dependent market
- 300+ cold rooms requiring continuous, reliable refrigeration
Solutions:
Similar stories
FoodTown sustains reliable refrigeration for large-scale food production in Brazil
FoodTown maintains stable, ultra-low-temperature refrigeration at its Osasco plant, supporting high-volume food production and nationwide distribution in Brazil.
Boehringer Ingelheim achieves 98% HVAC availability at its Campinas manufacturing plant
Boehringer Ingelheim improved HVAC reliability and achieved 98% equipment availability at its Campinas, Brazil plant, supporting compliance and pharmaceutical production.
UK data center improves energy efficiency by 8%
A UK data center advanced its long-term PUE strategy by increasing chilled plant efficiency and improving PUE to 1.296. Using OpenBlue digital solutions, the team identified hidden inefficiencies and achieved £38,000 in annual savings while maintaining performance for mission-critical operations.
Large-scale semiconductor cleanroom delivered in Singapore
A semiconductor manufacturer partnered with Johnson Controls to deliver a 24,000 sqm cleanroom in 18 months, meeting strict energy efficiency and reliability requirements.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)