- Johnson Controls
- Customer Success Stories
- The Grace, Westport Estate delivers luxury hospitality with intelligent fire safety
The Grace, Westport Estate delivers luxury hospitality with intelligent fire safety
Creating a seamless guest experience through advanced fire detection solutions
Impact Highlights
SafeLINC provides real-time visibility of alarms and system events.
More than 1,500 fire detection devices monitored across the property.
Intelligent cause-and-effect programming helps reduce unnecessary evacuations and guest disruption.
Modernising fire protection for a luxury guest environment
As part of the hotel's full refurbishment, the existing fire alarm infrastructure no longer aligned with current fire safety standards and the performance expectations of a modern luxury hospitality environment. Much of the legacy system consisted of ageing devices, outdated wiring and a traditional one-out, all-out evacuation approach that could trigger disruption across the entire property.
For a hotel hosting weddings, leisure guests, international visitors and high-profile dignitaries, unnecessary alarms and building-wide evacuations posed a significant risk to guest satisfaction and reputation. The project team needed a solution that would provide early warning detection while enabling a more intelligent response strategy.
This required a complete redesign of the system architecture, careful planning of panel locations, system coverage and integration with key building systems across the estate.
Creating a connected and intelligent fire detection platform
Working closely with the client, design team and electrical contractor, APM Securities designed and installed a fully rewired FireClass Fire Detection System built around three networked FireClass FC700 Series panels. The panels were strategically distributed across the main hotel, the kitchens and function spaces, and the luxury spa and leisure centre.
The FireClass platform enabled the team to support longer device circuits and a greater number of connected devices, helping reduce infrastructure requirements and associated costs for cabling, loop cards, power supplies and batteries. Advanced cause-and-effect programming allows staff to receive targeted alerts, investigate incidents quickly and take appropriate action before an event escalates into a full evacuation, reducing disruption for guests.
The solution incorporates SafeLINC remote connectivity, giving operational teams, maintenance personnel and service providers immediate visibility of alarms, pre-alarms and system events. Faster awareness and response help prevent minor incidents from escalating, while allowing many situations to be managed discreetly in the background before guests are affected.
Integration with HVAC (heating, ventilation and air conditioning) and the hotel's ANSUL® Restaurant Fire Suppression System from Johnson Controls further enhances response capabilities. The scalable design supports future connectivity across additional buildings within the wider Westport House Estate.
The system includes zone maps loaded directly onto the touchscreen interfaces of the FireClass panels, enabling staff to quickly identify the precise location of an alarm within the building. This enhanced situational awareness supports faster investigation and response times while helping teams manage incidents more effectively.
Enhancing safety, efficiency and guest experience
The new FireClass solution delivers far more than regulatory compliance. By combining intelligent, reliable detection with advanced notification and sophisticated cause-and-effect programming, the hotel can minimise disruption while maintaining the highest standards of life safety.
Staff now receive actionable information directly through SafeLINC remote monitoring tools, allowing them to investigate and resolve issues before they impact guests. During periods of unusually high temperatures, for example, pre-alarm notifications helped identify plant equipment performance issues before they developed into larger operational concerns.
The design has improved service efficiency for maintenance and support teams. With detailed event visibility available remotely across more than 1,500 fire detection devices, the hotel benefits from greater operational insight, reduced downtime and a more streamlined ownership experience.
“The FireClass FC700 Series panels are the best on the market. The power of the FireClass system allowed us to design a solution that not only delivers life safety and compliance but also improves the guest experience. The visibility provided through remote notifications means issues can be identified and addressed quickly, helping staff respond before problems impact hotel operations.”
Nathan Kearns, APM Securities
About The Grace, Westport Estate
“The support from John Murphy and the Johnson Controls team was second to none. They provided the information we needed when we needed it, and their responsiveness and attention to detail gave us confidence throughout the project. Their support throughout the project reassured us that we could deliver the right solution for a demanding luxury hospitality environment.”
Nathan Kearns, APM Securities
About the facility
- Luxury hotel within historic Westport House Estate
- 129 guestrooms, suites, spa and event facilities
- Refurbished destination focused on exceptional guest experiences
Solutions:
Similar stories
University stadium upgrades fire and emergency communication systems
University stadium enhances occupant safety with fire panels, speaker strobes and amber strobes to improve visibility and response.
Major Airport in the Pacific Northwest Modernizes Fire Protection Systems
A major Pacific Northwest airport upgraded its fire and passenger safety infrastructure, improving maintainability, emergency communications, and readiness for future expansion.
Protecting over 600,000 artifacts at Mexico City’s National Museum of Anthropology
Advanced fire detection and clean-agent suppression systems safeguard one of Latin America’s most important cultural collections while supporting safety and compliance.
Fire Protection for Frasers Group’s Automated Warehouse
Frasers Group implemented a bespoke fire detection and extinguishment system to safeguard its 13,000 m² automated warehouse and maintain operational continuity.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)